Required Materials
- A. Flir Lepton® & Lepton Breakout board
- B. Raspberry Pi
- C. CanaKit A Power Supply for Raspberry Pi (Or a powerful enough Micro USB charger)
- H. Computer Monitor with HDMI Port
- I. HDMI Cable
- J. Power Cable for Monitor
- K. USB Mouse
- L. USB Keyboard
The following items are required, but included in the CanaKit Raspberry Pi GPIO Breakout Board Bundle:
- D. Breadboard
- E. Wires
- F. CanaKit GPIO Breakout Board
- G. Ribbon Cable
Setting up the breadboard
1 Take out the Canakit GPIO Breakout Board and it’s ribbon cable from it’s plastic bag and
remove it from pink foam.
2 Attach Breakout Board to ribbon cable as shown.
3 Place Breakout Board onto breadboard as shown.
4 From the bundle of wires, select the following colors as shown. Colors can be interchanged
as long as you have the same number of wires for that color. (Example: photo shows 2 yellow wires, can be changed
with 2 of any other color)
5 Attach the wires from the breakout board to the following rows (as labeled) Follow the
pictures shown for gudiance. The key below shows where the pins go: (From breakout board to row #)
6 Key:
- a. White wire: Row (left) to Row (right)
- b. Yellow : Row (right) to Row (right)
- c. Yellow : Row (right) to Row (right)
- d. Blue Wire : Row (right) to Row (right)
- e. Black Wire: On row of holes next to red bar (right) to Row (right)
- f. Red Wire: On row of holes next to blue bar (right) to Row (right)
- g. Green Wire: Row (right) to Row (right)
- h. Blue Wire : Row (right) to Row (right)
When you’re all done, this is how it will look. Detailed steps to get this final appearance follow below.
Follow the pictures in order to assemble breadboard:
Attach the second yellow wire:
7 Attach Lepton camera to bread board such that it is facing outwards and that the pins
occupy rows 1-8 as shown below.
Setting up the Raspberry Pi
1 Gather materials.
2 Plug in the Monitor to a wall outlet using the monitor’s power cable and turn it on.
3 Take out your raspberry pi.
4 Check the slot underneath it to make sure the mini SD card is in place as shown in the
picture.
5 Attach Raspberry Pi to Monitor via HDMI cable.
6 Attach mouse and keyboard to Raspberry Pi by plugging them into the Pi’s USB ports.
7 Attach power cable to Raspberry Pi and plug it into a wall outlet. Your Pi should turn on
and take you to the desktop.
8 Click “Menu” in the top-left hand corner of the screen. Then, hover the mouse over
“Accessories” and another menu will appear. Select “Terminal” and a black terminal should appear in the middle of the
screen.
9 Type in the following commands in order EXACTLY as shown below. After you type each one,
press enter to ‘run’ that command.
sudo apt-get -y install git
git clone https://github.com/groupgets/LeptonModule.git
cd LeptonModule
cd raspberrypi_video
qmake && make
To explain what we did there, we grabbed the code from ‘github’, navigated to that folder and compiled it.
10 Remove top of Raspberry Pi and attach ribbon cable to the pins inside and make sure It is
pressed all the way down.
11 Type in the following command then press “Enter”.
a. sudo ./raspberrypi_video
12 Your Demo is setup and running! You can demo FCC functionality by pressing the “Perform
FCC” function. The shutter on the Lepton should click and screen should recalibrate the color.
Troubleshooting
If your screen does not display the infrared feed from the camera, attempt the following things:
- Unplug the ribbon cable from the Raspberry Pi and plug it back in without turning anything off/on.
- If you have multiple cameras try swapping a different camera into the Pi.